FIQ SGI IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FIQ SGI IMX6

880 Views
ailtonlopes
Contributor III

Hi.
Im trying to generate a fiq interruption for an SGI and the FIQ_Handler function is never called. 

I wanted to ask what could i be doing wrong??

First i created an SGI as  secure, using non-secure i get the right result with the IRQ but i wanted to use FIQ to handle the SGI when the interruption is defined as secure.
I even tried to redirect the FIQ exception to the Monitor mode but it doesn't work so i was thinking that maybe is something that i forgot to do before generating the SGI.
In other words my question could be how do you define that the secure interruptions will be redirected to the FIQ handler and non-secure to the IRQ. 

Kind Regards.

Ailton Lopes

Labels (2)
0 Kudos
1 Reply

563 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ailton

please look at fiq patch on

i.MX6 AVB Demo Implementation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos