Jtag on I.mx rt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jtag on I.mx rt

1,505 Views
snirr
Contributor I

Hello,

I'm designing a project base on I.mx rt 1050.

I saw the jtag configuration in the EVM, I'll like to create my own jtag connected directly to the i.mx rt instead of using mk20 for that.

Can I use the pinout configuration by segger J-link 9 pin cortex M adapter?

This is the link for the cortex M adapter of seger:

9-Pin Cortex M Adapter | SEGGER - The Embedded Experts 

Thanks,

Snir

Tags (1)
0 Kudos
1 Reply

747 Views
igorpadykov
NXP Employee
NXP Employee

Hi Snir

yes seems it can be used, RT1050 EVK debug interface is described in

sect.2.12. JTAG Connector MIMXRT1050 EVK Board Hardware User’s Guide
(swd is supported)
https://www.nxp.com/docs/en/user-guide/MIMXRT1050EVKHUG.pdf
jtag usage is described on

MCUXpresso IDE V10.1.0 with i.MX RT1052 Crossover Processor | MCU on Eclipse 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos