AnsweredAssumed Answered

PM Resume using Touch in i.MX6

Question asked by Anjalik Krishna on Jan 12, 2018
Latest reply on Jan 16, 2018 by Anjalik Krishna

Hi All,

  I am doing Power Management in my Linux code where the wakeup source is keypad and resistive touch. The touch driver is STMPE811 and basically the touch is working fine. Its a 4-wire touch controller with an interrupt line and no dedicated wakeup line . When I issue the command for suspend, the stmpe suspend function is called and the irq is enabled . The irq number is 275 and the touch interrupt number is also same. I tried adding wakeup-source property under stmpe node in dts file but the touch wakeup is not working and the system is under suspend mode.

 

When we probed the interrupt line using a multimeter probe, the moment the positive terminal of the multimeter  is touched on the interrupt line, the system is resumed . That looked little strange and confusing.

 

Could anyone help me to find out the solution to configure the touch as wakeup source ?

Outcomes