External circuitry required for USB0_PWR_FAULT in LPC4367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External circuitry required for USB0_PWR_FAULT in LPC4367

1,699 Views
akhilesh_sreedh
Contributor III

Hello,

The datasheet of LPC4367 provides USB0_PWR_FAULT functionality with the description "Port power fault signal indicating overcurrent condition; this signal monitors over-current on the USB bus (external circuitry required to detect over-current condition)." What exact external circuitry is required, is there any document or application note for the external circuit?  

Thanks

Akhilesh

Labels (2)
Tags (2)
0 Kudos
1 Reply

350 Views
soledad
NXP Employee
NXP Employee

Hi,

You can use the LPC4330-Xplorer Board schematic file as reference

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------