AnsweredAssumed Answered

PN7462 RX optimization for ISO14443A

Question asked by Bjorn De Smet on Jan 12, 2018
Latest reply on Jan 15, 2018 by IvanRuiz

I'm trying to optimize the PN7462 RX parameters (RxHpcf, RxGain and MinLevel) for ISO14443A card detection and communication. I have a few questions about this:

- Is there a documented procedure to do this?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during technology detection, collision resolution and activation?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during ISO14443A communication at 106 kbps?

Outcomes