Hi guys,
I'm working an imx6ull board and murata device type 1DX and i have some issues while using nxp linux release rel_imx_4.9.x_1.0.0_ga.
First of all i have tested the murata on linux version rel_imx_4.1.15_2.0.0 and everything was working fine. I upated the linux version to 4.9.x and the murata firmware also by downloading the correct one (4.9.11) on NXP website. The bcmdhd driver has been initialized correctly and i have issue with "HT clock" while trying to use wpa_supplicant to apply settings on wlan0 and to put it up by using this command :
wpa_supplicant -i wlan0 -Dnl80211 -c /etc/wpa_supplicant.conf -B&
I have attached all log files.
Issue log :
dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail request error: retried 20 times. UNRECOVERABLE!
dhd_net_bus_devreset: dhd_bus_devreset: -1
dhd_open : wl_android_wifi_on failed (-1)
wl_android_wifi_off in
dhd_prot_ioctl : bus is down. we have nothing to do
dhd_net_bus_devreset: dhd_bus_devreset: -35
Could not set interface wlan0 flags (UP): Operation not permitted
nl80211: Could not set interface 'wlan0' UP
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: Failed to initialize driver interface
Is somebody has an idea?
Best regards
Jean Gardy
Hi Jean,
in this case the problem will be the Murata drivers, so you may contact Murata to get the appropriate drivers.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------