AnsweredAssumed Answered

Error: The image creation script

Question asked by niranjanbc on Jan 10, 2018
Latest reply on Jan 12, 2018 by niranjanbc

i have build working fine on two Linux PC's and failing one PC. same source and yocto build.

what could be the issue.

 

NOTE: Running image creation script for tar: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.tar ...
NOTE: Creating symlinks for squashfs image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.squashfs -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.squashfs
NOTE: Creating symlinks for ext3 image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.ext3 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.ext3
NOTE: Creating symlinks for tar image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.tar.bz2 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.tar.bz2
NOTE: Running image creation script for sdcard: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard ...
ERROR: Error: The image creation script '/home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard' returned 1:
0+0 records in
0+0 records out
0 bytes (0 B) copied, 2.083e-05 s, 0.0 kB/s
Model: (file)
Disk /home/niranjan/fsl-community-bsp/build_emmc/tmp/deploy/images/phx-core-pca/core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.sdcard: 302MB
Sector size (logical/physical): 512B/512B
Partition Table: msdos
Disk Flags:

Number Start End Size Type File system Flags
1 4194kB 12.6MB 8389kB primary lba
2 12.6MB 298MB 285MB primary

758+0 records in
758+0 records out
388096 bytes (388 kB) copied, 0.000897308 s, 433 MB/s
mkfs.vfat 2.11 (12 Mar 2005)
WARNING: exit code 1 from a shell command.

DEBUG: Python function do_rootfs finished
ERROR: Function failed: do_rootfs

Outcomes