AnsweredAssumed Answered

Problem with cold boot i.MX287

Question asked by Lorenzo Roldan Melero on Jan 10, 2018
Latest reply on Feb 8, 2018 by igorpadykov

We have two iMX287 based platform, heavily inspired by the iMX28 EVK-RevD. One DDR2 memory W971GG6kB251 (Winbond) and nand TC58NVG1S3ETAi0.

 

We problem that we have in both platform is that if we boot in low temperature (-5 / 10ºC) we have some crc error at descompressing linux Kernel.

 

We are tried to power supply the board only with 5V, Only with Batt or dual mode.

 

When the temperatura up to 15ºC the boot of the board is normal and it works fine.

 

Any idea?

 

Thanks in advance

Best reards

Lorenzo  

Outcomes