PMIC test in u boot for IMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC test in u boot for IMX6UL

956 Views
anshulkhare
Contributor III

Hello All,

Good day to you!

My requirement is to test PMIC (PFUZE3000) in u boot for IMX6UL board.

The pmic command is enabled and working in u-boot.

What test I can perform on PMIC? for eg: can we read the voltage values?

Could anyone kindly provide us with some information on this. Any help on this is much appreciated.

Thank you. 

Labels (2)
0 Kudos
3 Replies

636 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anshul 

one can look at examples in uboot:

pmic_reg_read() in function power_init_board() in uboot/board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6ul_14x14_evk/mx6ul_1...

and add custom functions for reading pmic registers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

636 Views
anshulkhare
Contributor III

HI igor,

Thanks for your reply.

Does pmic command in u boot do the same thing?

"pmic read" allows to read values from the registers.

Is there any way we can read voltage values?

0 Kudos

636 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anshul 

there is no way to read voltages as  PFUZE3000 does not

have adc, only registers.

Best regards
igor

0 Kudos