AnsweredAssumed Answered

writing to text segment in flash cause hard fault

Question asked by roymessinger on Jan 9, 2018
Latest reply on Jan 23, 2018 by Butcher

(I've moved this question from my original thread and decided to open a new one...)

I'm using a K64 on custom board and KBOOT (but it happened also when putting the app on address zero, without Kboot). When writing to a new defined section in the text segment of the flash a hard fault is caused.

My code snippet is as follows:

 

include...
#ifdef __cplusplus
extern "C" {
#endif
uint16_t __attribute__((section (".MyappFlag"))) appFlag = 0xBEEF;\\after this line is executed all is well and appFlag is changed to BEEF. I see it with breakpoints.


int main(void) {
appFlag = 1; \\after this line is executed the hard fault occurs.
BOARD_BootClockRUN();
Board_Init_UART();
Board_InitLEDs();
Board_Inputs();
Board_Outputs();

 

 

the linker file which cause it is as follows:

MEMORY
{
m_interrupts (RX) : ORIGIN = 0x0000A000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x0000A400, LENGTH = 0x000FFBF0 - 0xA400 - 0x100
appFlag (RX) : ORIGIN = 0xFFAF0, LENGTH = 0x100    \* 0xFFAF0 = FFBF0 - 100. But doesn't matter what is the size of the flag, and I tried various addresses. always hard fault*/
m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00030000
}

/* Define output sections */
SECTIONS
{

.my_section :
{
. = ALIGN(4);
KEEP(*(.MyappFlag)) /* keep my variable even if not referenced */
. = ALIGN(4);
} > appFlag

 

when writing the linker in that way (accessing the RAM and not the ROM-writing the appFlag to m_data_2) it works fine, but then the bin file size is huge (I guess because 0x20020000 =~512MB):

 

MEMORY
{
m_interrupts (RX) : ORIGIN = 0x0000A000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x0000A400, LENGTH = 0x00075C00
m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00030000
}

/* placing appFlag section at given address:*/
.my_section 0x20020000 :
{

. = ALIGN(4);

KEEP(*(.MyappFlag)) /* keep my variable even if not referenced */

. = ALIGN(4);

} > m_data_2

 

 

Code size:

arm-none-eabi-size --format=berkeley -x --totals "BCA2.elf"
text           data      bss     dec    hex    filename
0x164f0 0x8d0 0x1344 98564 18104 BCA2.elf
0x164f0 0x8d0 0x1344 98564 18104 (TOTALS)

 

 

Any ideas?

Outcomes