AnsweredAssumed Answered

Devkit Motor GD Application not working.

Question asked by Krishna Chaitanya Devulapalli on Jan 8, 2018
Latest reply on Jan 8, 2018 by dumitru-daniel.popa

I was trying to build a motor control application with S32K144 and Devkit Motor GD. But it is not working. I connected the power supply to the Devkit board. When is do this and build the model from simulink, it is being built successfully but I cannot see any voltage values in Freemaster. I also tried observing the Phase Voltage and Hall Voltage readings using a Voltmeter but I could not see any values. There is no problem with the motor since I used it for different applications using different board. Should I connect power to both the boards or is there any other solution? 

Outcomes