Hi everyone,
When I active the ccp mode in the 5643l configuration block,then generator the code.And Getting the a2l file from canape asap2editor.Then use canape to calibration.But when I send message to the controller,the controller do not response.Then I use PE to debug,I set breakpoint in the 'ccpCommand((uint8_t*)temp);'.When I use canape send message to the controller,
the program do not goto the code.The program in the annex.
Hi zenghongjin@chegustech.com,
Before enabling the CCP - have you checked if your CAN networks works?
What i meant to say is: if you configure the MPC5643L to broadcast a CAN message (let's say with a a counter value) can you see that message over the CAN ?
Thank you!
Daniel
I am sure the CAN network working.Because I transmit a message through busmaster,meanwhile I can see the message in the window.In this case,The CAN network do not display a error message.
I see, but i was referring to the CAN on the MPC5643L.
Inside the toolbox there is a CAN example. Does it works on your setup. Can you receive the messages sent from MPC5643L into the Busmaster ?
Hope this helps!
Daniel
After I download the can_simple_block.mdl to the controller,then I use busmaster to observe the message.The message I can receive in the window.