AnsweredAssumed Answered

Timing violation of i.MXUL SPI communication

Question asked by Surendra Jadhav on Jan 7, 2018
Latest reply on Jan 8, 2018 by igorpadykov

Hi,

 

We have connected SPI-UART chip on SPI interface of i.MX6UL, which can work up to 26MHz.

However its working fine till 10MHz and after this frequency we are not able to communicate with SPI-UART chip.

Though the waveform quality is not much degraded, we feel that its issue related to set up and hold time violation. Please confirm.

 

SPI-UART chip has MOSI hold time is min 3ns and MOSI setup time is min 5ns.

Do we have provision in iMX6UL with which we can match these timings to avoid the timing violation. Do we have programmable setup and hold time in i.MX6UL.+

 

Regards,

Surendra

Outcomes