hellow sir,
recently i joined the industry so i want to know that how to write a boot-up or start-up file for freescale t1040 with u-boot ??
Solved! Go to Solution.
U-boot is boot loader. It contains start-up code.
Usually modification of u-boot configuration is enough for using a new board. Configuration of the u-boot is available in the following folder in u-boot source: /include/configs/.
See attached file.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Usually the following command sequence is used for SDK installing under Ubuntu 14:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
This command sequence provides u-boot generation.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
U-boot is boot loader. It contains start-up code.
Usually modification of u-boot configuration is enough for using a new board. Configuration of the u-boot is available in the following folder in u-boot source: /include/configs/.
See attached file.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sir this contain only Header file. Can i get whole boot loader for RDBT1040.
Thank You