PTN3392BS FIRMWARE UPGRADE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3392BS FIRMWARE UPGRADE

Jump to solution
856 Views
andrewatkinson
Contributor I

Hi we are working with a military Head Worn Display which requires 600x800 VGA converted from

DP++ using the PTN3392BS on our processor reader board. We are having trouble forcing low res VGA to the display due to the lack of I2C signalling. Other eader boards we make can do this utilising a second vendor adaptor changing onboard DP++ to VGA.

Do you have the latest firmware version for the PTN3392BS and directions on how to flash it.

 Thanks for your help...Andrew

#firmware update

0 Kudos
1 Solution
716 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Andrew,

 

Unfortunately, firmware (or details about it) for the PTN3392 cannot be shared without a signed NDA, you may need to contact your NXP sales representative to get such information. However, it is guaranteed that the part number PTN3392BS/F4Y contains the latest version of the firmware (Firmware 4.0).

 

Have a great day,

Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
717 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Andrew,

 

Unfortunately, firmware (or details about it) for the PTN3392 cannot be shared without a signed NDA, you may need to contact your NXP sales representative to get such information. However, it is guaranteed that the part number PTN3392BS/F4Y contains the latest version of the firmware (Firmware 4.0).

 

Have a great day,

Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------