Hi, i have started work on a project that requires the use of the USB host CDC. I am trying to make the example found in the SDK work with my device.
I am using the SDK 2.3.0 with MCUXpresso IDE.
The example i am trying to use is the host_cdc_bm.
When debugging, plugging my device on the K66F board, i see that it is detected:
The console prints:
device cdc attached:
pid=0x2018vid=0x3eb address=1
cdc device attached
But when i try to send data to it, i get kStatus_USB_TransferFailed in the USB_HostCdcDataInCallback. From what i can understand so far this is cause by a timeout. But i can't figure out why this is happening.
Usb is kind of new to me, any help in figuring this issue would be greatly appreciated.
Thank you
Hello Daniel
Here is what i see in the console:
Whatever i type in the console is not echoed back.
i tried to follow the code to see where it breaks, and what i found is that i get a kStatus_USB_TransferFailed
in the USB_HostCdcDataOutCallback and USB_HostCdcDataInCallback
From what i understand of the code, this seems to indicate that no byte where transfered, but i am not sure why.
Any help would be greatly appreciated!
Hi Christian:
Have you solved this issue? I just did a quick test with this demo. Frdm-k66 as a usb cdc host, and TWR-K65 as a usb cdc device. It works on my end. please see below picture. What's you settings?
Regards
Daniel