AnsweredAssumed Answered

JN-AN-1171: Missing header files and includes

Question asked by Siegfried Som on Jan 3, 2018
Latest reply on Jan 9, 2018 by Mario Ignacio Castaneda Lopez

Hello,


I have installed the BeyondStudio for NXP (JN-SW-4141) and the SDK JN-SW-4168 as described in the User Guide JN-UG-3098. I then imported the application note JN-AN-1171. My workspace is located in a different directory, which is why I did the steps described in Appendix B as well.

 

I corrected a wrong reference on the include path "C: \NXP\bstudio_nxp\sdk\sdk\JN-SW-4166\Components\Common\Include"to... 4168....

 

A reference is also made to an include directory "/ZCL Library/Include" in the workspace path, which does not exist in the project?

 

Some of the header files in the source code, like "zps_gen. h" and "dbg.h" I can't find them on my hard drive?

 

I've been trying to find the mistake for some time now. Can someone tell me what I'm doing wrong?

 

Where can I find the two ZigBee plugins whose installation is described in chapter 1.2.3 of the JN-UG-3098?

 

I hope someone can help me.

 

Best regards

Sigi

 

Outcomes