Hello mario_castaneda,
I am facing problem in PDM EEPROM.
when i tried to load data in EEPROM its works correctly.
but after a reboot while reading "PDM_eReadDataFromRecord" this API,
it shows " PDM_E_STATUS_INVLD_PARAM".
how to overcome this problem.
Best Regards,
Dheeraj Sawant
Hi Dheeraj,
Application data records in EEPROM can be read by the application using the function PDM_eReadDataFromRecord(). The record to be read is specified using its 16-bit identifier and a data buffer in RAM must also be specified in which the read data will be stored.
If the call to PDM_eReadDataFromRecord() indicates that the record has not been found, the application should also call PDM_eDeleteAllData() because another application may have been running that does not use the same record ID but has written inconsistent ZigBee PRO records to the PDM module
Regards,
Mario