S32 Design Studio for Apple Mac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Apple Mac

2,019 Views
edgarmichel
Contributor II

Actually S32 Design Studio is available for Windows/Linux. Is there a port for Apple Mac available eg as Eclipse plugin?

Labels (1)
2 Replies

1,610 Views
ajgar17374
Contributor I

I am using a MacBook Air 13 inch notebook and I am disappointed with the fact that S32 Design Studio IDE is not supported by MAC. You can go for byd studio as it is supported by Macbook as well as in your  iPad but don't try force installing or any other methods as once I tried and my MacBook Air  Won't Turn On and then I have to send it for repair  

0 Kudos

1,610 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is no version of S32DS for MAC. As a workaround you can use virtual machine (VMware, VirtualBOX...) on your Apple machine.

Jiri

0 Kudos