913+964+imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

913+964+imx6q

1,082 Views
yabinzhang
Contributor I

用的版本内核是3.14.28,硬件是ds90ub913+ds90ub964+imx6q,相关的patch已经打上了。

问题:四路视频已成功抓到,摄像头输出的1280x720@25fps,摄像头模组的场信号已经测试过为25Hz,也就是说硬件没有问题。正常是1s中抓到25帧,现在我2s中才抓到25帧。请问下各位工程师们,IPU底层是不是需要特殊的处理才不会丢帧,或者各位给个建议怎么去处理这个问题。

Labels (1)
0 Kudos
2 Replies

796 Views
liuzheng
Contributor I

你好在哪里能得到913+964+imx6q 的patch,目前项目想移植到jetson_tx2上,如果方便的话请回复到215781344@qq.com ;万分感激 

0 Kudos

796 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Yabin,

      无论你使用的是PCIe接口还是MIPI CSI-2接口,IPU和VPU处理4路1280x720,都是很困难的。你尝试把分辨率配置为720x576@25帧,这是D1的标准分辨率和帧率。应该没问题的。

Have a nice day!

TIC weidong sun

0 Kudos