Dear, All:
I am developing the SRIO application of T2080, so I wanna refer to the SRA application code.
And I can not find it in SDK, where can I find it?
ps:My SDK is "QorIQ Linux SDK v2.0 SOURCE", and it says:
"10.7.16.1.2.2 SDK Installation
SRA is based on NXP Linux SDK. So to use SRA, make sure NXP Linux SDK is well installed."
Looking forward to your reply and thanks!
Solved! Go to Solution.
Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------