Can sb_loader support I.MX6 or other similar manufacturing tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can sb_loader support I.MX6 or other similar manufacturing tools

Jump to solution
871 Views
geekdarcy
Contributor III
Hi everyone,
 
I'm developing a new board based on the IMX6q.
First,My custom board had passed memory stress test via "NXP DDR Test Tool".
I'm trying to load my custom  u-boot to ram by sb_loader executable and I get the following output:
$sb_loader.exe -f u-boot.bin
->Executed plugin successfully.
->Succeed to download u-boot.bin to the device.
->Failed to run plugin u-boot.bin to the device.

I get sb_loader from  Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER.

And how to get some debug info on the debug UART

Does anyone know what I am doing wrong? Any clue about that error?
 
Kind regards
Labels (2)
1 Solution
574 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

also may be useful to check sb_loader usage on

i.MX USB Loader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
574 Views
geekdarcy
Contributor III

Hi everyone,

I had load my custom u-boot.bin to ram successfully by  using  sb_loader.v1.2.

微信截图_20171228153304.png

->DCD Write Success!

->Executed plugin successfully.

 ->Loading Firmware.

->Succeed to download u-boot.bin to the device.

->Run into the image successfully.

thanks .

0 Kudos
575 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

also may be useful to check sb_loader usage on

i.MX USB Loader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------