Hello team,
I am using iMx6QP SABRE-AI board for which i am connecting muRata Type ZQ EVK. Wifi adapter connected on SDIO2 and BT signals connected on J32.
I am able to finish the boot process and enter the root login.
When i use the command "insmod /lib/modules/3.14.52-1.1.0_ga+g5f6f0a5/kernel/drivers/net/wireless/bcmdhd/bcmdhd.ko firmware_path=/lib/firmware/bcm/ZQ_BCM89335/fw_bcmdhd.bin nvram_path=/lib/firmware/bcm/ZQ_BCM89335/bcmdhd.ZQ.OOB.cal dhd_msg_level=0x1" -> i am facing an error "failed to powerup DHD generic adapter".
Can someone help me on this to bringup Wifi at first?
Please let me know if any other detail needed.
Note: Attached kernel log FYR.
Thank you.
Hi Shyam
please install broadcom firmware package for i.MX Linux L3.14.52 BSP
https://www.nxp.com/webapp/Download?colCode=BCMDHD-L3_14_52&appType=license
if this will not help one can try to obtain updated firmware for BCM89335 module from murata support
link: wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------