MXP121 keyboard programmed no keys depressed, power off, "some keys" pressed with power up and original data that was written is overridden with the "some keys" data. Need help with registers, filters, read, write?
Hi Tripp,
I recommend you to test it using our suggested initialization code:
#define TouchThre 10 //15//30//10
#define ReleaThre 6 //8//25//8
void MPR121_init(void)
{
//Reset MPR121 if not reset correctly
IIC_ByteWrite(0x80,0x63); //Soft reset
IIC_ByteWrite(0x5E,0x00); //Stop mode
//touch pad baseline filter
//rising
IIC_ByteWrite(0x2B,0x01); // MAX HALF DELTA Rising
IIC_ByteWrite(0x2C,0x01); // NOISE HALF DELTA Rising
IIC_ByteWrite(0x2D,0x0E); // NOISE COUNT LIMIT Rising
IIC_ByteWrite(0x2E,0x00); // DELAY LIMIT Rising
//falling
IIC_ByteWrite(0x2F,0x01); // MAX HALF DELTA Falling
IIC_ByteWrite(0x30,0x05); // NOISE HALF DELTA Falling
IIC_ByteWrite(0x31,0x01); // NOISE COUNT LIMIT Falling
IIC_ByteWrite(0x32,0x00); // DELAY LIMIT Falling
//touched
IIC_ByteWrite(0x33,0x00); // Noise half delta touched
IIC_ByteWrite(0x34,0x00); // Noise counts touched
IIC_ByteWrite(0x35,0x00); // Filter delay touched
//Touch pad threshold
IIC_ByteWrite(0x41,TouchThre); // ELE0 TOUCH THRESHOLD
IIC_ByteWrite(0x42,ReleaThre); // ELE0 RELEASE THRESHOLD
IIC_ByteWrite(0x43,TouchThre); // ELE1 TOUCH THRESHOLD
IIC_ByteWrite(0x44,ReleaThre); // ELE1 RELEASE THRESHOLD
IIC_ByteWrite(0x45,TouchThre); // ELE2 TOUCH THRESHOLD
IIC_ByteWrite(0x46,ReleaThre); // ELE2 RELEASE THRESHOLD
IIC_ByteWrite(0x47,TouchThre); // ELE3 TOUCH THRESHOLD
IIC_ByteWrite(0x48,ReleaThre); // ELE3 RELEASE THRESHOLD
IIC_ByteWrite(0x49,TouchThre); // ELE4 TOUCH THRESHOLD
IIC_ByteWrite(0x4A,ReleaThre); // ELE4 RELEASE THRESHOLD
IIC_ByteWrite(0x4B,TouchThre); // ELE5 TOUCH THRESHOLD
IIC_ByteWrite(0x4C,ReleaThre); // ELE5 RELEASE THRESHOLD
IIC_ByteWrite(0x4D,TouchThre); // ELE6 TOUCH THRESHOLD
IIC_ByteWrite(0x4E,ReleaThre); // ELE6 RELEASE THRESHOLD
IIC_ByteWrite(0x4F,TouchThre); // ELE7 TOUCH THRESHOLD
IIC_ByteWrite(0x50,ReleaThre); // ELE7 RELEASE THRESHOLD
IIC_ByteWrite(0x51,TouchThre); // ELE8 TOUCH THRESHOLD
IIC_ByteWrite(0x52,ReleaThre); // ELE8 RELEASE THRESHOLD
IIC_ByteWrite(0x53,TouchThre); // ELE9 TOUCH THRESHOLD
IIC_ByteWrite(0x54,ReleaThre); // ELE9 RELEASE THRESHOLD
IIC_ByteWrite(0x55,TouchThre); // ELE10 TOUCH THRESHOLD
IIC_ByteWrite(0x56,ReleaThre); // ELE10 RELEASE THRESHOLD
IIC_ByteWrite(0x57,TouchThre); // ELE11 TOUCH THRESHOLD
IIC_ByteWrite(0x58,ReleaThre); // ELE11 RELEASE THRESHOLD
//touch /release debounce
IIC_ByteWrite(0x5B,0x00);
// response time = SFI(10) X ESI(8ms) = 80ms
IIC_ByteWrite(0x5D,0x13);
//FFI=18
IIC_ByteWrite(0x5C,0x80);
//Auto configuration
IIC_ByteWrite(0x7B,0x8F);
// charge to 70% of Vdd , high sensitivity
IIC_ByteWrite(0x7D,0xE4);
IIC_ByteWrite(0x7E,0x94);
IIC_ByteWrite(0x7F,0xCD);
// 12 electrodes enabled
IIC_ByteWrite(0x5E,0xCC);
}
Regarding the communication I recommend you to check the application note AN3895 from the following link: https://www.nxp.com/docs/en/application-note/AN3895.pdf
And also recommend you to read the application note AN3890 which includes information about how to improve the capability of a filtering system for the MPR121: https://www.nxp.com/docs/en/application-note/AN3890.pdf
Regards,
Jose
NXP Semiconductor
MPR121 is the controller in question.