Start Up configuration of PMIC MC32PF3000A2EP for IMX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Start Up configuration of PMIC MC32PF3000A2EP for IMX7D

370 Views
logeshs
Contributor II

Hi, 

We used MC32PF3000A2EP in our one of the IOT products. 

In that as per datasheet Page 35 and the Table 42. Start-up configuration clarity is required. 

The confusion is between default configuration and Pre Programmed OTP configuration. 

1. MC32PF3000A2 (A2 series part supports our required configuration votlages) customized start-up configuration directly from the factory? Or we need to program the chip ? 

2. At first power on , the chip is it in the default configuration or pre programmed OTP configuration? What will be the output voltages for the part MC32PF3000A2EP ? 

Thanks,

Logesh

 

 

 

Labels (1)
0 Kudos
1 Reply

290 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.

  The MC32PF3000A2 is factory pre-programmed part.

 

2.

  The chip (A2) is in the pre-programmed OTP configuration at first power on.

 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos