AnsweredAssumed Answered

USB Host examples on LPCXpresso546xx - RevC

Question asked by Andrew Fisher on Dec 15, 2017
Latest reply on Dec 20, 2017 by Hui_Ma

Hello,

 

I have an LPCXpresso546xx RevC board with an LPC54628 chip on it. I have been trying to get USB host working but am having no success with the MCUXpresso 3.2.0 SDK examples.

 

I can get device examples working no problem but the host examples all say "host init done" and then sit there doing nothing. Putting breakpoints at various points eg. the kUSB_HostEventAttatch case never trigger.

 

I have used various leads and tried various examples. I can see the High Speed port powers up but that is it.

 

Has anyone else seen these examples work?

 

Also it is not clear to me how I would configure these examples to run on the Full speed interface (as will eventually be needing). The device examples are all obvious in the usb_device_config.h file.

 

Andy

Outcomes