Power consumption of STOP mode for S9KEAZ64AMLH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power consumption of STOP mode for S9KEAZ64AMLH

2,152 Views
zhouwoniu
Contributor I

大家好!我的芯片是S9KEAZ64AMLH,进入stop模式后电流260ua。软件上没有使用任何外设,硬件上只保留了MCU。使用官网的例程,进入stop配置如下:
/* PMC Initialization */
    PMC_ConfigType  PMC_Config={{0}};

    PMC_Config.sCtrlstatus.bits.bBandgapEn = 1;        /* Enable Bandgap buffer */
    PMC_Config.sCtrlstatus.bits.bLvdStopEn = 0;        /* Disable Low-Voltage Detect(LVD) in Stop mode */
    PMC_Config.sCtrlstatus.bits.bLvdRstEn = 0;        /* LVD events do not generate hardware resets. */

    PMC_Init(PMC, &PMC_Config);                                        /* Initialization of PMC */
    PMC_DisableLVWInterrupt(PMC);                                /* Disable hardware interrupt requests for LVWF */
    uint8_t Ch = PMC_GetLVWFlag(PMC);                                        /* Get the lvw warning flag */

    PMC_SetMode(PMC,PmcModeStop3);                                /* Enable PMC in stop mode */

请问还有什么需要注意的?

Labels (1)
0 Kudos
5 Replies

1,818 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi woniu,

请问你有测试过关闭Bandgap、关闭LVD状态下STOP的电流吗?

260uA这个电流应该过高了。

Best Regards,

Robin

0 Kudos

1,818 Views
zhouwoniu
Contributor I

现在测试的条件是关闭了LVD的。请问Bandgap是什么?

0 Kudos

1,818 Views
fupeng
Contributor II

你好,电流降下去了么?

0 Kudos

1,818 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

请参考这篇帖子实现STOP模式下获得uA级电流吧:

how to achieve the KEA128 lowest static current in STOP mode

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,818 Views
zhouwoniu
Contributor I

请问NXP的工程师在没?

0 Kudos