Hi.
I am using a MPC5777C with a MPC57XX Motherboard Rev C.
I tried to configure the FEC using the last configuration indicated on Questions of MPC5777C FEC setting.
The microcontroller is transmitting a simple packet and ARP request packets too.
Using the wireshark, with the ETH board in promiscuous mode , the data cannot be received.
The micro controller receive wrongly the packets generated by the host computer ( size and type )
When I used the loopback indicated on post Problems about receiving ethernet frame on MPC5604E the microcontroller could receive the ARP packets transmitted.
The clock configuration is the same as Example MPC5777C-PinToggleStationery GHS714
I am using a MPC57xx MB Rev C,
The Jumper Configuration
J26 is 1-2.
J510 is 1-2.
J514 is 2-3.
Is there any other missing configuration can cause its problem ?
It is possible share any example like Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP PHY for MPC5777C using the PHY of the motherboard?
Thanks.