THE sdk v0.8.4 error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

THE sdk v0.8.4 error

904 Views
zhanhui
Contributor II

In the S32DS V2.0 with the S32K144_SDK 0.8.4,the example “ftm_periodic_interrupt_s32k144” it has error,like this:

   pastedImage_1.png

 the SDK didn't has the HAL driver ,and in the compoents library it also has the hal driver, but in the S32DS V1.3 with the SDK RTM 1.00,it has the hal driver. 

0 Kudos
2 Replies

745 Views
xmwang
Contributor II

FTM_DRV_ClearTimerOverflow()

0 Kudos

745 Views
zhanhui
Contributor II

So the example code is a bug to use the FTM_HAL? 

0 Kudos