Hello all,
I have an LPC11u68 LpcExpresso board and I have uploaded the attached cpp file (via creating a new project and verifying it runs correctly). My program wishes to hold a pin low even through power cycles of the LPC board. As you can see from the attached sketch I have put a pulldown via pin muxing on pin 1_18 and I tell the system to make it output low.
The problem is, when I power up the board there is a very brief period where the pin goes high just as the power goes high, then the pin goes low as it should. Is there a way to keep that pin low even during power application to the board? It is a requirement for a project I am working on.
In the attached scope shot, the (Yellow) Channel 1 is pin 1_18 and the (Blue) Channel 2 is the 3.3V line to show when power is applied.
Thank you for your help,
Dustin
Hi Dustin Hagstrom,
It's no way to modify the default state of pin: pull-up enabled before execute the corresponding instruction.
Hope this is clear.
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------