AnsweredAssumed Answered

Boot Animation taking too long on iMX6

Question asked by Suhas Kaundinya on Nov 30, 2017
Latest reply on Dec 5, 2017 by Diego Adrian Cuevas

Hello,

 

I am using i.MX 6Quad SABRE-AI with Andriod N.

The boot animation log is as follows, but it is taking 42 seconds to boot. Is there a way I can shorten the time? Is there a problem in the log? Also, how to change the permissions?

 

init: Starting service 'bootanim'...
type=1400 audit(12.610:14): avc: denied { getattr } for pid=299 comm="bootanimation1
type=1400 audit(14.520:15): avc: denied { write } for pid=377 comm="BootAnimation" 1
type=1400 audit(14.540:16): avc: denied { open } for pid=377 comm="BootAnimation" p1
capability: warning: `main' uses 32-bit capabilities (legacy support in use)
period 0 ,timeout is 0, wake up is : 0
period 0 ,timeout is 0, wake up is : 0
acc_open
acc_release
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
period 66 ,timeout is 0, wake up is : 0
mma enable setting active
init: Service 'bootanim' (pid 299) exited with status 0

 

Regards,

Suhas

Outcomes