Hi
I have working with yocto to generate the recipe for bluebox mini. I have the application that uses qt4 and for that I have written a recipe. Everything goes fine e.g. cmake, make etc but when it links to qt4 it links to wrong sysroots: This is what it shows:
/Yocto_EAR2.0/QorIQ-SDK-V2.0-20160527-yocto/build_ls2084abbmini/tmp/sysroots/x86_64-linux/usr/lib/libQtGui.so: error adding symbols: File in wrong format
it should rather links to
/Yocto_EAR2.0/QorIQ-SDK-V2.0-20160527-yocto/build_ls2084abbmini/tmp/sysroots/ls2084abbmini/usr/lib/libQtGui.so:
Any fix for that?
Pradeep