When i using mcu expresso config toolv4 for imxrt 1050 ,it give error selected processor does not contain about supported sdk components.
Hello ,
Do you choose the MCUXpresso IDE when download SDK package ?
If yes,the newest version MCUXpresso IDE v10.1.0 integrated the configure tools,so the standalone Configure tools doesn't includes MCUXpresso IDE.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Sir,
I am downloaded IMX RT 1050 SDK with all toolchains.So,how can i use with IAR and Keil and solve this problem.
Hello,
support for RT1050 in Config Tools is currently limited to Pins tool.
'sdk_components.xml' are needed for proper integration with toolchain project, which is currently not supported yet, but it will be added soon. In the mean time, you can use the tool without integration with toolchain project.
Also support for clock tool is planned.
Regards
Marek
Is there any update on when Config tools will support CLOCK?
thanks
Bobcat
Robert,
The clock data for the MCUXpresso Config Tools is now available. If you computer is connected to the internet the Config Tools will be able to retrieve the new clock data.
Thanks for letting me know, Clark.
It doesn't seem to be available to me yet. Could you tell me how to access it?
I'm using "MCU Xpresso IDE / Help / Check for updates" with no results.
I also browsed to the downloads here, and it's still showing a 2017 download as the most recent:
Hi Robert,
Which chip ? Please have a look at this table, it shows the supported configure tools with different chips:
MCUXpresso Supported Devices Table
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Robert, I was told it will be available in next couple of days.
Regards
Marek