sabresd_6dq android_N7.1.2_2.0.0 boota: bad boot image magic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sabresd_6dq android_N7.1.2_2.0.0 boota: bad boot image magic

971 Views
ebrahimshaik
Contributor I

U-Boot 2017.03 (Nov 28 2017 - 17:36:59 +0530)

CPU:   Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 27C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
flash target is MMC:1
Net:   
Warning: ethernet@02188000 using MAC address from ROM
eth0: ethernet@02188000 [PRIME]
Fastboot: Normal
Hit any key to stop autoboot:  0
boota mmc1
boota: bad boot image magic
USB EHCI 1.00

0 Kudos
2 Replies

626 Views
igorpadykov
NXP Employee
NXP Employee

Hi ebrahim

"bad image magic" may mean that wrong (for other board) image was used.

Please try Demo Images

https://www.nxp.com/webapp/Download?colCode=IMX_N7.1.2_2.0.0_ANDROID_DEMO_SD_BSP&appType=license&loc... 

and use MFG Tool for that release for programming image

i.MX 6/7D Series Manufacturing Toolkit for Android N7.1.2_2.0.0 Release

https://www.nxp.com/webapp/Download?colCode=IMX_N7.1.2_2.0.0_TOOL&appType=license&location=null 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

626 Views
ebrahimshaik
Contributor I

After reboot system it is working now.

0 Kudos