why imx6  so easy be burned?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why imx6  so easy be burned?

489 Views
zhanghan
Contributor II

power.png my power is +24V,after transform as pic above ,then use MMPF0100F0ZES to generate the power for imx6 use,Once without  power down,I unplug my power port,but quickly I plug my power port on with power ,then i find the imx6 can not work .and the  LIGHT OF D1DYT.png is weak,then I change another  new imx6 ,then  the board run normally.CAN somebody tell me why?

Labels (1)
0 Kudos
1 Reply

398 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

quickly plugging my power off on violates processor power-up sequence as

power supplies should be applied in sequence from fully unpowered

(no any remaining voltages) processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos