About an internal protection diode of i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About an internal protection diode of i.MX6DL

Jump to solution
671 Views
yuuki
Senior Contributor II

Dear all,

Would you tell me about an internal protection diode of GPIO pin (NANDF_CS1: C16)?

Does GPIO pin have an internal protection diode?

If it is Yes, Would you tell me the allowable maximum current?

Best Regards,

Yuuki

Labels (1)
0 Kudos
1 Solution
570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes there are internal protection diodes, max. current is not specified

by datasheet, in general not recommended to exceed 1mA.

Best regards
igor
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
571 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes there are internal protection diodes, max. current is not specified

by datasheet, in general not recommended to exceed 1mA.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos