windriver和Multlink驱动显示错误

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

windriver和Multlink驱动显示错误

1,213 Views
kuozhang
Contributor I

我安装了CW10.6之前还是可以正常使用(一天前),今天连接PE USB Multlink interface 时出现连接不上的情况,打开设备管理器,显示如截图的情况,我不知道是什么原因。我百度了一下,说是驱动的原因,我更新了驱动但是显示还是如截图2所示,

是不是要重新安装CW10.6呢?还是其他什么原因?

希望能够得到帮助,这个对我很重要。

Labels (1)
0 Kudos
1 Reply

985 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kuo Zhang

I suggest you
1. right click on "USB Multilink 2.0" and "WinDriver", then uninstall these driver.
2. disconnect board the reconnect it. again windows will search driver and reinstall it. please wait for several minutes. check Jungo in Device Manager, see if the drivers are installed now.
3. If still can not be installed, download and install
http://www.pemicro.com/downloads/main_downloads_temp/201711241213386979854/PEDrivers_install.exe
then restart computer and try steps 1-2

Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos