Ernest Snaith

SPI with manual SS (MC9S12XDT512 - MC33810)

Discussion created by Ernest Snaith on Sep 29, 2008
Latest reply on Sep 29, 2008 by Ernest Snaith
Is it possible to have manual control of the SS pin while using SPI. I would like to interface with a 16 bit SPI devise (MC33810) where the SS signal is required but it must not return to idle between transmission of the two bytes. I have seen this devise used with the same microcontroller so there is presumably a way of doing it but i dont have access to the code.
 
Cheers
 
 
 
 

Outcomes