AnsweredAssumed Answered

iMX6S CSI0 16-bit YCbCr capture: one color channel data missing

Question asked by Pavel Azizov on Nov 20, 2017
Latest reply on Nov 21, 2017 by igorpadykov

Hello.

 

I capture signal from FPGA on iMX6solo CSI0.

I use data pins D19~D4. I have also configured all necessary pins in *.dts-file.

Input data format: 16-bit parallel YUYV (YUV422).

 

I have prepared my own camera driver with the following parameters:

    my_capture_data.pix.pixelformat = V4L2_PIX_FMT_YUYV;
    my_capture_data.pix.width = 1024;
    my_capture_data.pix.height = 768;

 

I have also changed data width in drivers/media/video/mxc/capture/mxc_v4l2_capture.c:

   csi_param.data_width = IPU_CSI_DATA_WIDTH_16;

 

I send an image with synthetic color data:

Y channel is from my image,

U channel is always 0x7F,

V channel is always 0x81.

 

I am able to capture the image and I see the following data:

Y 0x7F Y 0 Y 0x7F Y 0 ...

 

Y channel data is in its place.

U channel data is in its place.

V channel is always 0.

 

What might be the issue?

Outcomes