AnsweredAssumed Answered

SATA can't work on LS2088ARDB+LSDK1709

Question asked by Jin Yanjiang on Nov 19, 2017
Latest reply on Jan 28, 2018 by Yiping Wang

Hi ,

 

According to "LSDK-KC-REV0.pdf", I have downloaded the pre-built image from nxp.com, and burn it on a LS2088ARDB board. The board can find the SATA disk during booting, but kernel reported some errors as below, then SATA can't work finally.

Did I miss anything?

 

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
 ata2.00: qc timeout (cmd 0xec)
ata2.00: failed to IDENTIFY (I/O error, err_mask=0x4)
ata2: limiting SATA link speed to 1.5 Gbps
ata2: SATA link up 1.5 Gbps (SStatus 113 SControl 310)
ata2.00: failed to IDENTIFY (I/O error, err_mask=0x100)
ata2: SATA link up 1.5 Gbps (SStatus 113 SControl 310

 

Software environment:

$ wget http://www.nxp.com/lgfiles/sdk/lsdk1709/firmware_ls2088ardb_uboot_norboot.img

 

Hardware environment:

 

Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 4

 

Full boot logs:

 

Please see attachment.

Attachments

Outcomes