Dear Engineers of NXP:
I am using the T2080RDB-PC board, and found a problem about the DDR.
I changed the DDR3 memory card(original=D3XP56082XL10AA)
with my laptop memory card(RMT3150ED58E8W1600).
Then, It doesn't work any more.
I have considered the 1.35V(DDR3L) and 1.5V(DDR3) , tried others laptop memory card(about five kinds of memory card), and get the same results.
I saw the register of DDR below, and it is fine!
I used the DDRv tool to validate them, and would't get the right value.
However, the original DDR3L works fine in 1066M/1333M/1600M/1866M, and could find the right value in DDRv tool.
I also tried the 4GB DDR3L laptop memory card, and It couldn't work too.
Theonly difference is that D3XP56082XL10AA support ECC and RMT3150ED58E8W1600 cann't support ECC...
Does the T2080RDB-PC only support the ECC memory card?Why my memory card can't work?
Looking forward to your reply, and Best wishes to you!
Yours sincerely
Solved! Go to Solution.
In the provided SO-DIMM datasheet it is written:
● 204-pin Dual-in-line DDR3 memory module.
● JEDEC Standard with 1.5 V (±0.075 V) power supply
Please provide U-Boot log and datasheet for the SO-DIMM in question.
Please provide the SO-DIMM datasheet.
In the provided SO-DIMM datasheet it is written:
● 204-pin Dual-in-line DDR3 memory module.
● JEDEC Standard with 1.5 V (±0.075 V) power supply