How to enable USB OTG for LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable USB OTG for LS1046A

692 Views
andreasgeißler
Contributor II

Hello,

We are currently try to use the #OTG feature for USB on the LS1046A. We have added:

- CONFIG_USB_DWC3_DUAL_ROLE=y

- CONFIG_USB_OTG=y

to the kernel defconfig and changed the dr_mode in the device tree to "otg".

When using the USB in "peripheral" mode the USB is working as a mass storage device as expected. but when using "otg" the USB port is not working as host or device.

What steps are needed to enable the OTG? What did we forget or did wrong?

Thanks!

Regards,

Andreas

Tags (1)
0 Kudos
1 Reply

452 Views
Pavel
NXP Employee
NXP Employee

Please wait answer on your technical case about this problem.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos