CAN FD 8Mbps not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN FD 8Mbps not working

1,385 Views
yalamandadosaky
Contributor V

Hi, I am using S32ds power pc v1.2 and MPC5748G EVB,I have successfully transmitted with CAN FD 1Mbps, 4Mbps but 8Mbps is not working. I have tried different baud rate settings

My baud rate settings are

.bitrate_cbt =

{

.propseg = 0,

.phaseseg1 = 1,

.phaseseg2 = 1,

.preDivider= 0,

.rJumbpwidth = 1

}

I have enabled TDC and offset value changed from 1 to 10 but still it didn't worked.

Can anyone help me to is there any problem with these settings or give me an idea how to resolve it.

3 Replies

967 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

see this thread, https://community.nxp.com/message/958035 

BR, Petr

967 Views
yalamandadosaky
Contributor V

Hi PetrS‌, Through Component inspector(processor Expert) I am unable to change the PE clock frequency to more than 40Mhz.

Is there any other way to select the more than 40Mhz clock frequency.

Thanks

0 Kudos

967 Views
PetrS
NXP TechSupport
NXP TechSupport

checking a MPC5748G DS/RM I see max FlexCAN PEclock could be 40Mhz. Thus max bitrate is 5Mhz.

BR, Petr