960-1215MHz is a broadband design. The optimum Zload and Zsource impedances depend on the frequency. Impedance matching for broadband design is more complex task and, most cases, the broadband design loses to narrow-band design in gain and efficiency. Typically, you have to use ADS optimization tool to achieve design targets.
In your case, the target bandwidth is 20MHz. It is a narrow-band design. You can perform impedance matching at the center of the operating frequency band. So, it is not reasonable to follow 960-1215MHz design for your task.
2.
>there is no complete circuit, you can provide here?
If needed, i can provide you the DXF file. Please, create a ticket to technical support. I'm not allowed to put this file at this community.
这里第2点提到,可以提供DXF的图纸给我,能否发到我邮箱呢?441400387@qq.com
Please create a Support Request to get DXF file.
Support|NXP