AnsweredAssumed Answered

Jennet-IP on JN5168, eJIP_AddTrap = E_JIP_ERROR_FAILED ?

Question asked by David Tolar on Nov 10, 2017
Latest reply on Nov 15, 2017 by David Tolar

Jennet-IP on JN5168 - please could somebody help me with usage of eJIP_AddTrap() function? It should set trap on specified local variable and the stack then send notifications to specified multicast address (JN-UG-3080, side 141). But the problem is that call to this function (eJIP_AddTrap) always returns with E_JIP_ERROR_FAILED. I checked parameters of the function and I can't see any issues (valid phMib, u8VarID, psAddr...). Maybe someone with access to source code of this function could tell me: what could be the reasons for returning this error code, what checks are done inside the function.

I'd be very happy if someone could help with this issue.

Best Regards, David

Outcomes