Hi Sir,
I am use imx6dq with android 6.0.1 and I do like update the image from SD card in recovery mode,
is there any information / guide for that?
B.R jerry
You need to set "recovery" insted of "boot" for booti option in u-boot configuration to enter recovery mode.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Victor,
Thanks for suggestion, I have booted to recovery mode and added the option "apply update from SD card" to recovery menu,
but system inform me that there no /scard detected even I put the image files on SD card which format fat or ext4, so I wonder if any guide
to mount SD card in recovery mode.