Hi,
Just bought my first freedom board: FRDM-KL28Z
I have several questions regarding the firmware update on this board.
In the product detail file it is written the following:
Daplink Mode: Interface
Interface Version: 0241
Bootloader Version: 0241
According with the mbed developer website I need to update the Daplink.
I downloaded the Daplink and also the binary file for the OpenSDA.
I read the firmware update procedure from here:
- OpenSDA Serial and Debug Adapter|NXP
...however it refers to the OpenSDA firmware update. It is not clear for me how I can update the Daplink...
- It is the same procedure like for the OpenSDA?
- Do I need to update both OpenSDA and Daplink?
- Do I need to unzip the Daplink file or simply put it as it is on zip format?
I would really appreciate if someone can further clarify this for me.
I also noticed that it is no SDK for this board. When downloading the SDK it points to the FRDM-KL27Z.
Any plans to release a SDK for this board too?
Thank you,
Hi Gheorghe Kobori
Answering your questions:
- It is the same procedure like for the OpenSDA?
you have to make the same steps like a OpenSDA interface update; plug the board with the reset button pressed, drag and drop the DAPLink rev0242 binary that you download in our page, disconnect it and connect it again.
- Do I need to update both OpenSDA and Daplink?
No, only the Daplink version, to the DAPLink rev0242
- Do I need to unzip the Daplink file or simply put it as it is on zip format?
You have to drag and drop the .bin file, it is named as k20dx_frdmkl28z_if_crc.bin
Any plans to release a SDK for this board too?
Actually, there is SDK for this board, SDK 2.2 in the SDK builder page:
Welcome to MCUXpresso | MCUXpresso Config Tools
Hope this information could help you.
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------