AnsweredAssumed Answered

Import debug configurations from "cloned" projects fails

Question asked by Lucas Magasweran on Nov 7, 2017
Latest reply on Nov 7, 2017 by Alice_Yang

How do I ensure the debug and launch configurations are imported automatically?

 

I used https://mcuxpresso.nxp.com/en/example-projects to clone the default bubble example for the FRDM-KL27Z for KSDK 2.2.1.

 

After extracting the archive, the project imports and builds using Kinetis Design Studio (KDS) 3.2.0 but the debug configurations do not get imported. I have to manually re-create them using the defaults (in my case JLink) but the "Machine name" is not set to "MKL27Z64xxx4".

 

I also tried importing from the command line using either "-import" or "-importAll" but neither work.

/opt/Freescale/KDS_v3/eclipse/kinetis-design-studio -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import /vagrant/bubble -data /vagrant/workspace

 

 

I also tried to import the "Launch Configurations" from the Import wizard but it simply deletes the .launch files from the project.

Outcomes