AnsweredAssumed Answered

BeyondStudio build process takes long time

Question asked by dostshah on Nov 2, 2017
Latest reply on Nov 14, 2017 by Castaneda Lopez

I am using beyond studio to build zigbeePro application. The build process is too slow. If a single file is modified it takes around 4+ minutes. For a clean and build of the ZigbeeControlBridge Sample code, the ide takes 35+ minutes.

 

The PC I am using is an i7 with around 8 GB Ram

 

Task Manager shows the following 

 

the content of bstudio_nxp.ini is as follows

plugins/org.eclipse.equinox.launcher_1.3.0.v20130327-1440.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.win32.win32.x86_1.1.200.v20130807-1835
-vmargs
-XX:MaxPermSize=768m
–Xmx768m

How can I solve this issue?

Outcomes