I install the CW10.7.2,and found most Demos named PSC913x,can these demos run on the BSC9132 board? what are the differences between BSC and PSC ? And when I want to use JTAG on BSC9132 board,is it support Codewarrior Tap,or only support USB tap?
PSC913x is renamed as BSC913x, demos for PSC913x also can run on BSC913x.
CodeWarrior TAP can be used on all QorIQ and Qonverge target boards, the old product USB TAP has not manufactured any more.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your answers! And is there any demo to show how to use the CONVPE with BSC9132 MAPLE?I found there has no any demo in CW10.7.2 to show how to use the CONVPE to do convolution and correlation.
Thank you for your answers!